TSX712 used in a Sallen-Key topology: issues with some capacitors packages Hi everybody,We are using TSX712 in a Sallen-key topology used as low-pass filter We haveC1, C2 = 1 uFR1,R2 = 1KVpsupp = 5VVin = sinusoidal signal with amplitude 4,5 Vpp, offset=2,5V, Freq = 60 HzVout is the expected one when using Capacitors package 0603inch rating-voltage = 50V ;using other kind of Capacitors (0201inch with rating-voltage 6,3 V or 0402inch with rating-voltage = 16 V)Vout has a distorsion in terms of an increasing gradient during increasing amplitude half-period and a decreasing gradient during decreasing amplitude half-period. So Vout sinusoidal time-offset to Vin is not constant (time-offset is decreasing during amplitude-increasing-half-period ; time-offset is increasing during amplitude-decreasing-half-period).Vin maximum value is occurring every half period (at about 8,3 msec)Vout maximum value is occurring before the half period (at about 7,4 msec)This different behaviour, related to used capacitors, is expected ? There are some restrictions