VL53L1X minimum time to to scan from standby I apologize I have not read ALL of the related documentation but have read enough to feel it may be hard to resolve this question:I would like to employ the VL53L1X to detect object flow, i.e. people, however as someone has already point out it requires continual scanning, hence consuming more power than a cordless/battery can provide over long period. So, I would like to use some other mechanism to detect a person in the area, e.g. sound, PIR, etc and then start scanning for flow from one zone to next. I have read about "hw standby" and "sw standby", as well as boot. But it's unclear the minimum duration of these and how they effect ability to start scanning and trying to determine flow. So...1) What is the the use/interpretation/timing of the HW standby?2) What is the minimum time to first scan (i.e. ranging of the in zone or out zone early enough to catch direction of low) when power is already applied, but XShut is used to "wake up" and start scan?3) What is the minimum time to fir