How to add feedback for all outputs? HI ,I have working on switched mode power supply design with wide input range (30-300) and I am using on the design many ST components.I have make my first design using eDesignSuite from ST using Viper37 IC, but I ordered only 2 IC and after that I couldn't find any Viper37 any more in any market, for that I used another IC with separately Moseft outside.When I designed multiple outputs smps on eDesignSuite it gives me only feedback from only one output as shown on the schematic below.After make the PCB of the design I test in the lab, and it works very well on no load condition but when I add load (resistors in parallel), the voltage of all the output voltage are decreasing.I have multiple output from the transformer with only one feedback for 24v output, I think the problem is having only one feedback for all systems for that it is not steady. I attached my circuit here, may you please show me how can I add feedback for all of my outputs ?sincerely,ZAIM