Why would STSPIN220 drive power to the outputs at initial power-on? To ask this question another way, what is expected at the output pins when Vs < 1.5V during power-up?I have a design for driving a linear actuator which uses the STSPIN220. My customer has an issue related to unexpected device power off, and those events correspond to power-on of the STSPIN220. During their investigation, they found significant voltage on the output pins immediately when the device is powered on (via a high-side FET to switch the voltage). While I can't confirm the behavior myself since I don't have hardware, I am told that there can be a voltage spike of >1V which occurs at the motor driver outputs, regardless of how STBY and EN are set. Part of the current working theory is that the driver is pulling signifcant current at this time, possibly due to both sides of the H-Bridge being enabled, and that is causing the regulator to drop-out. As far as the STSPIN220, it's been speculated that there is a point at which the outputs are powered before the threshold