Can all SPC582B60E1C(0, D, G or H) output CAN on pins 61 and 62 (PAD[44] and PAD[45])? Hello everyone,I looked into DS11597 Rev 4 datasheet (page 104) and the mentioned TN1263 (SPC582Bx IO definition: Signal description and input multiplexing tables) documents, but I could not figure out, whether the SPC582B60E1Cx with 3 (x=0,D) CAN interfaces is able to output CAN4_sys1 peripheral. I need CAN output on the pins 61 and 62 (i.e., PC12 and PC13 or PAD[44] and PAD[45]).I assume, that the 0 and D version only has CAN0_sys0,CAN1_sys0,CAN2_sys0, am I right?In the SPC5 Studio it seems as if I can only use the version with 7 CAN interfaces.Could you tell me, how to select the version with 3 CAN interfaces in the PinMap Editor?Is it possible to get samples of the SPC582B60E1CG or ..CH or ..MG or ..MH?Thank you very much for your answers in advance.Best regards,Christopher Seifert