I would like to change the "Image of Image widget" on receiving the different status
Hello All,
I am using "STM32746G-DISCO" Kit.
I am using the "Image widget" to display the image.
I would like to change the "Image" on fix location on receiving the "CONNECT" & "DISCONNECT" status.
I am using two different Image for CONNECT & DISCONNECT.
Can you please guide me how do i update the image on receiving the "CONNECT" & "DISCONNECT" Status.
I am using following API but when it run, It freeze the GUI.
if(status == 1)
{
image1.setXY(3.76);
Image1.SetBitmap(Bitmap(BITMAP_CONNECTED_ID));
add(Image1);
}
else if(status == 2)
{
image1.setXY(3.76);
Image1.SetBitmap(Bitmap(BITMAP_DISCONNECTED_ID));
add(Image1);
}
please, Do needful for me.
Regards,
Nikunj Patel