EVAL6480H-DISC and quadrature encoder application
Hi all,
for a stepper based application I've to link the frequency that came from a quadrature encoder to the driving speed of a bipolar stepper motor. This board is equipped by a STM32F105RB processor, I've read inside the RM0008 (the reference manual) that the counter can be configured to act as Encoder Interface (§14.3.16 pag 329/1132). I some trouble to found the pins on this board related the timer that should be theoretically usedto perform the quadrature counter (if some are not directly accessible I'll wire up to perform the testing). From the reference manual these input are called TI1 and TI2 but at what physical pin are associated and where I can found this information?
[SOLVED]
Looking inside the RM0008 Reference Manual (Rev. 19) on page 294/1132 at the Figure 52 all became clear.

Thank for now!
Best regards
Fabio