Associate II
June 7, 2018
Solved
CubeMX I2C Configuration issue with STM32H753IIKx
- June 7, 2018
- 1 reply
- 1579 views
Posted on June 07, 2018 at 12:55
Hello,
I've created new STM32H753IIKx project with CubeMX(Ver4.26.0), and changed the I2C1/I2C2 setting into 'I2C' from 'Disable' in Pinout tab.
And, switch to Configuration tab, open the I2C1 Configuration, move to GPIO Settings tab, I can modify the Fast Mode setting to 'Enable' from 'Disable' on each PB8/PB9.
However, in the I2C2 Configuration case, I cannot modify the Fast Mode setting that shows 'n/a'.
Does this mean that I2C2 cannot be used as Fast Mode ?
Is there difference between I2C1 and I2C2 from functionality point of view ?
Thanks.
Shirane