Skip to main content
NDesh.2
Associate II
June 30, 2022
Solved

Is STM32L431KBU6 available in 5V supply? We want to just changed existing part with 5V so that can avoid level shifting of SPI signals(Work on 5V).

  • June 30, 2022
  • 5 replies
  • 4856 views

..

This topic has been closed for replies.
Best answer by NDesh.2

Issue resolved. we have used Buffer IC to level shift the voltage levels so continuing with same uC.

5 replies

Michal Dudka
Lead
June 30, 2022

As far as i know, there is none 5V STM32. But most of STM32 have 5V tolerant inputs. That means you can connect external 5V signals directly to STM pin. You can also transmit 5V signals by "open drain" GPIO output mode with external pullup to 5V, but speed wil be limited (depending on pullup value and wiring capacity).

NDesh.2
NDesh.2Author
Associate II
July 1, 2022

Thanks for your response.

Actually I want to drive SPI slave from STM32 uC (Master) .This STM32L431KBU6 works on 3.3V & Slave circuit works on 5V.To avoid money in level shifter IC for this I was just looking for same uC specification with just supply voltage 5V.

As you suggested I know for MISO signal this will be easily done but for all other three lines(CS,SCK,MOSI) by just pull up is it possible to do that?

Michal Dudka
Lead
July 1, 2022

It depends on communication speed and trace lengths. Generally it is possible. But communication speed is limited on short distances (few centimeters) to typicaly hunderds of kbit/s. Simply look into datasheet and find some "5V tolerant pin". Connect wire same length like you plan to use and pullup to 5V - start with 1kOhm for example. Init it as "Open drain" then toggle with that pin, and look on oscilloscope at rising and falling edge durations. Then you can estimate achievable birates. Then you can possibly decrease pullup value to reach faster edges and higher bitrates. But pullup value is limited into minimal value about 5V/20mA=270R and in that case, communication can take significat total current (3 signals, 20mA each). It's better to hold on values in range 1k or higher if it is possible. And of course, in meantime between communication, you should keep output pins in High to conserve power.

Andrew Neil
Super User
June 30, 2022

@NDesh.2​  -What does the datasheet tell you?

@Michal Dudka​ "most of STM32 have 5V tolerant inputs"

To be more precise, most STM32 have some 5V-tolerant pins.

Again, full details will be in the datasheet.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NDesh.2
NDesh.2Author
Associate II
July 1, 2022

In datasheet it is mentioned as 3.3V or max 3.6V.

But as my product is ready & SW is ready with STM32L431KBU6 uC, just as cost saving view (Remove level shifter IC) & to have all IC's on same voltage(+5V), I am looking for same uC with only supply working voltage as +5V.

I was asking this because generally manufacture like ATMEL produces same uC with variants who works on 3.3V & 5V.

Andrew Neil
Super User
July 1, 2022

@NDesh.2​ "generally manufacture like ATMEL produces same uC with variants who works on 3.3V & 5V"

Actually, they don't - very few manufacturers have 5V Cortex-M microcontrollers.

IIRC, Microchip (formerly Atmel) has only one?

EDIT:

0693W00000QKFyUQAX.png

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KnarfB
Super User
July 1, 2022

There is no chip variant, but you can read all about 5V tolerant GPIO in AN4899 Application note "STM32 microcontroller GPIO hardware settings and low-power consumption"

hth

KnarfB

Andrew Neil
Super User
July 1, 2022

Have you tried the "STM32 Finder new mobile app" ?

https://www.st.com/en/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus.html#st-highlight-promotion

EDIT

Or the Product Selector?

0693W00000QKG22QAH.png 

Although that seems to be broken at the moment:

0693W00000QKG1iQAH.png

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Amel NASRI
ST Technical Moderator
July 18, 2022

Hi @Andrew Neil​ ,

Do you still have the issue with "MCU portfolio and selection" please?

There is no such issue on my side.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
July 18, 2022

@Amel NASRI​ - seems to be OK now.

@NDesh.2​ - did it work for you?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NDesh.2
NDesh.2Author
Associate II
July 19, 2022

Thanks All for your support!!!

Andrew Neil
Super User
July 19, 2022

You're e welcome. Please help the community by marking the solution:

0693W000008y9fZQAQ.png

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.