Skip to main content
Associate II
May 29, 2025
Question

LED blink works with CFG_DEBUGGER enabled but not when disabled on STM32WB5MM-DK

  • May 29, 2025
  • 5 replies
  • 615 views

I’m developing a custom BLE server on an STM32WB5MM-DK using STM32CubeWB HAL, the Sequencer (UTIL_SEQ), and the HW TimeServer (HW_TS) for periodic tasks. I implemented a repeated LED blink.

  • With CFG_DEBUGGER_SUPPORTED set to 1, the LED toggles on/off every ~5 s as expected.

  • With CFG_DEBUGGER_SUPPORTED set to 0, the LED never blinks, though BLE advertising and characteristic updates continue.

I’ve tuned low-power settings and task scheduling, but the OFF callback (and thus the blink sequence) never runs when CFG_DEBUGGER_SUPPORTED is off. I suspect there is something wrong between Stop mode and the Sequencer/timers, but can’t pinpoint the issue.

/* In Custom_APP_Init(): register tasks & create timers */
UTIL_SEQ_RegTask(1 << CFG_TASK_LEDON, UTIL_SEQ_RFU, LEDONTask);
UTIL_SEQ_RegTask(1 << CFG_TASK_LEDOFF, UTIL_SEQ_RFU, LEDOFFTask);

HW_TS_Create(CFG_TIM_LEDON_ISR, &Custom_App_Context.LEDON_TIMER_ID,
 hw_ts_Repeated, LEDON_TIMER_ISR);
HW_TS_Create(CFG_TIM_LEDOFF_ISR, &Custom_App_Context.LEDOFF_TIMER_ID,
 hw_ts_SingleShot, LEDOFF_TIMER_ISR);

/* Kick off the blink loop on init */
HW_TS_Start(Custom_App_Context.LEDON_TIMER_ID, LEDONTIMER_INTERVAL);

/* Timer ISRs: queue the corresponding tasks */
void LEDON_TIMER_ISR(void)
{
 UTIL_SEQ_SetTask(1 << CFG_TASK_LEDON, CFG_SCH_PRIO_1);
}

void LEDOFF_TIMER_ISR(void)
{
 HW_TS_Stop(Custom_App_Context.LEDOFF_TIMER_ID);
 UTIL_SEQ_SetTask(1 << CFG_TASK_LEDOFF, CFG_SCH_PRIO_1);
}
/* LED on: disable Stop mode, set LED, schedule off */
void LEDONTask(void)
{
 UTIL_LPM_SetStopMode(CFG_LPM_APP_BLE, UTIL_LPM_DISABLE);
 APP_DBG_MSG("LEDONTask");
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
 HW_TS_Start(Custom_App_Context.LEDOFF_TIMER_ID, LEDOFFTIMER_INTERVAL);
}

/* LED off: clear LED, re-enable Stop mode */
void LEDOFFTask(void)
{
 APP_DBG_MSG("LEDOFFTask");
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
 UTIL_LPM_SetStopMode(CFG_LPM_APP_BLE, UTIL_LPM_ENABLE);
}



 

5 replies

FilipKremen
ST Employee
May 29, 2025

Hello,

could you please share the project?

Thank you.

Best regards,

ST support

Associate II
May 29, 2025

@FilipKremen wrote:

Hello,

could you please share the project?

Thank you.

Best regards,

ST support


Hi Filip,
Here is the zip file:

Tesla DeLorean
Guru
May 29, 2025

Make sure you're explicitly enabling the GPIOA clock when you enable / setup the pin.

Perhaps dump the register settings to a console / output, independently of the debugger.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
FilipKremen
ST Employee
May 30, 2025

Hello,

did you change anything else? I tried your project, and I can see pin toggling with or without CFG_DEBUGGER_SUPPORTED.

Best regards,

ST support

Associate II
May 30, 2025

Hi Filip,

did you enable LPM. I think it has something to do with low power mode. 
When I enable low power mode. The LED doesn’t toggle. 
thanks. 

FilipKremen
ST Employee
May 30, 2025

Hello,

I noticed you enabled standby mode during initialization. It should be disabled in MX_APPE_Init() function.

Please note that if you want to enter standby mode, the radio must be turned off. Please have a look at this topic here as it can be helpful for your implementation.

Solved: Re: Problem with entering standby mode in STM32WB5... - STMicroelectronics Community

void MX_APPE_Init(void)
{
 System_Init(); /**< System initialization */

 SystemPower_Config(); /**< Configure the system Power Mode */

 HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */

/* USER CODE BEGIN APPE_Init_1 */
 APPD_Init();

 UTIL_LPM_SetOffMode(1U << CFG_LPM_APP, UTIL_LPM_DISABLE);
/* USER CODE END APPE_Init_1 */
 appe_Tl_Init();	/* Initialize all transport layers */

 /**
 * From now, the application is waiting for the ready event (VS_HCI_C2_Ready)
 * received on the system channel before starting the Stack
 * This system event is received with APPE_SysUserEvtRx()
 */
/* USER CODE BEGIN APPE_Init_2 */

/* USER CODE END APPE_Init_2 */

 return;
}

Best regards,

ST support

Associate II
May 30, 2025

Hi Filip,
I updated the code according to your recommendation but the GPIO still doesnt toggle.
I have reuploaded the file again, could you please review.
Thanks

FilipKremen
ST Employee
May 30, 2025

Hello,

please try to comment this line __HAL_RCC_GPIOA_CLK_DISABLE() in APPD_Init(). This function disables the clock for GPIOA. Let me know if it works on your side, thank you.

Best regards,

ST support