SPC58NN cannot debug after flash DCF Debug tool:Lauterbach Software Version: R.2018.02.000096069The screenshot of CMM is as follows:Of course, this cmm is modified by the cmm of the MPC5xxx chipThe above script writes two addresses,0x00400360, the write data is 0x05AA55AF000000000x00400368, the write data is 0x0000030100080000 (start offline bist)After executing the cmm, the debugger shows debug port fail.And the lower right corner of trace32 jumps reset from time to timeI also learned about an official cmm from the "AN4939 How to run self-test in the SPC58NN84x device Rev2 March 2019.pdf" document, but I can't find this cmm on the official website, can you tell me where to download it?So far, the above has happened to two boards, so desperately hope someone understands what happened and can let me know.Best regards!