X-NUCLEO-GNSS1A1 / LIV3F enabling NMEA 4.10 possible? Hello,I don't understand whether it is possible or not to enable NMEA 4.10 messages on the X-NUCLEO-GNSS1A1 / LIV3F. I'm currently testing it with the updated firmware version, as per $$PSTMVER,GNSSLIB_8.4.10.16.3_ARM*5E. This is confusing, because in this post (edited in July 2022):https://community.st.com/s/feed/0D50X0000AIcA9mSQFFrancesco Virlinzi shares that it is indeed possible on the Teseo-LIV3F, by entering (and after that saving and restarting):$PSTMSETPAR,1122,0x02($PSTMSETPAR,1122,0x04 would restore it to V3.01)However, I'm using the device configured as Galileo-only: and the following initial time should signal that it is, in fact, the case:$$GPTXT,DEFAULT LIV CONFIGURATION*2B$$GPZDA,000001.50,03,09,2017,00,00*6CAs I am not seeing the corrisponding TalkerID change to GA (instead of GP), I'm assuming that such change has not happened. In section 11.4.7 of the UM2229 - Rev 5 Software Manual (November 2021), when describing the --ZDA sentence, you find the following:Synopsis f